FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency setting
FAQ
Frequency setting
Do I have to press the "SET" key when setting the frequency with the setting dial?
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
You need to press the "SET" key with the initial setting.
The frequency is not set unless you press the "SET" key.
Setting Pr.161 (Frequency setting/key lock operation selection) to "1" activates the potentiometer mode and the inverter operates at the frequency set by the setting dial without pressing the "SET" key.
(The frequency setting value is memorized in approximately 10 seconds after it becomes stable after being set by the setting dial.)
The frequency is not set unless you press the "SET" key.
Setting Pr.161 (Frequency setting/key lock operation selection) to "1" activates the potentiometer mode and the inverter operates at the frequency set by the setting dial without pressing the "SET" key.
(The frequency setting value is memorized in approximately 10 seconds after it becomes stable after being set by the setting dial.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700