Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21740
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I input voltage of 0 to 10 V between external terminals 4 and 5 to set the frequency.
I have already changed the DIP switch setting on the board and set Pr.267 (Terminal 4 input selection) to "2".
The voltage between the terminals 4 and 5 is measured as 10 V, and the percent value of C7 (Terminal 4 frequency setting gain) is read as "101.0%". I want to set it to "100%".
Can I set it?
Category : 

Answer

Since the percent value read by the calibration parameter C7 indicates that the voltage of 10 V is internally detected as 101.0%, use 101.0% as is.
If you change it to 100% unjustly, the setting frequency may rise.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?