FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Auto tuning
FAQ
Auto tuning
When I set Pr.96 (Auto tuning setting/status) to "1", "96" and "1" flicker alternately. What should I do next?
- Category :
Answer
If you have already set other parameters necessary for tuning (Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, and Pr.84), press the MODE button to return to the frequency monitor window.
You will notice that "1" is shown. ("1" is not shown if auto tuning is not set.)
Sending the start command after that starts auto tuning.
Indication proceeds from "1", "2", and "3", and auto tuning completes. Turn off the start command.
You will notice that "1" is shown. ("1" is not shown if auto tuning is not set.)
Sending the start command after that starts auto tuning.
Indication proceeds from "1", "2", and "3", and auto tuning completes. Turn off the start command.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700