FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Parameter
FAQ
Parameter
Is there any parameter that can be used to change the time before an overload trip (electronic thermal O/L relay error) occurs?
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
No parameter can be used to directly set this time.
Changing Pr.9 (Electronic thermal O/L relay) changes the time.
Changing Pr.9 (Electronic thermal O/L relay) changes the time.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700