FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Current setting
FAQ
Current setting
I want to use the external terminal 4 and use the inverter with current input 4 to 20 mA. The initial frequency settings are 0 Hz for 4 mA and 60 Hz for 20 mA. Can I switch the setting? (Setting of 60 Hz for 4 mA, 0 Hz for 20 mA)
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
Yes.
The parameters used when the terminal 4 is used are C5, C6, 126, and C7.
Set Pr.C5 (Terminal 4 frequency setting bias frequency) while feeding a current signal of 4 mA.
Change the frequency to 60 Hz for this time. Also, set Pr.C6 (Terminal 4 frequency setting bias) in this state. (Reading Pr.C6 shows a value close to 20.)
Then, set Pr.126 (Terminal 4 frequency setting gain frequency) while feeding a current signal of 20 mA.
Change the frequency to 0 Hz for this time.
Also, set Pr.C7 (Terminal 4 frequency setting gain) in this state. (Reading Pr.C7 shows a value very close to 100.)
The parameters used when the terminal 4 is used are C5, C6, 126, and C7.
Set Pr.C5 (Terminal 4 frequency setting bias frequency) while feeding a current signal of 4 mA.
Change the frequency to 60 Hz for this time. Also, set Pr.C6 (Terminal 4 frequency setting bias) in this state. (Reading Pr.C6 shows a value close to 20.)
Then, set Pr.126 (Terminal 4 frequency setting gain frequency) while feeding a current signal of 20 mA.
Change the frequency to 0 Hz for this time.
Also, set Pr.C7 (Terminal 4 frequency setting gain) in this state. (Reading Pr.C7 shows a value very close to 100.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700