FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Operation panel LED
FAQ
Operation panel LED
I try to operate the inverter by inputting the start signal from the external terminal STF-SD and set the frequency using the setting dial.
For Pr.79 (Operation mode), "3" is set.
The operation panel LEDs "MON", "PU", "EXT", and "RUN" are lit. Is this OK?
For Pr.79 (Operation mode), "3" is set.
The operation panel LEDs "MON", "PU", "EXT", and "RUN" are lit. Is this OK?
- Category :
Answer
No problem.
LEDs "PU" and "EXT" indicate that Pr.79 is set to "3".
"MON" indicates that the operation status is monitored.
"RUN" indicates that the inverter is operating.
LEDs "PU" and "EXT" indicate that Pr.79 is set to "3".
"MON" indicates that the operation status is monitored.
"RUN" indicates that the inverter is operating.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ