FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
What should I do not to operate the motor below a low speed (5 Hz)?
What happens if I set Pr.13 to "60 Hz", and the frequency to 30 Hz?
What happens if I set Pr.13 to "60 Hz", and the frequency to 30 Hz?
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
Set Pr.13 (Starting frequency) or Pr.2 (Lower limit) to "5 Hz".
Also set Pr.10 (DC injection brake operation frequency) to "5 Hz".
The inverter does not operate if the starting frequency is 60 Hz and the setting frequency is 30 Hz.
Also set Pr.10 (DC injection brake operation frequency) to "5 Hz".
The inverter does not operate if the starting frequency is 60 Hz and the setting frequency is 30 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700