FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency setting
FAQ
Frequency setting
I use an external potentiometer to give frequency commands. What happens if the frequency commands from the potentiometer cease?
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
When the potentiometer is disconnected and frequency commands cease, the input potential becomes around 0 V.
Therefore, the frequency command becomes analog-calibrated frequency around 0 V.
Therefore, the frequency command becomes analog-calibrated frequency around 0 V.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700