FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Frequency setting
FAQ
Frequency setting
I use the previous option AS-OX (manual controller) externally.
However, the readings of the output frequency meter and monitor indicator meter do not match.
How should I configure the inverter?
However, the readings of the output frequency meter and monitor indicator meter do not match.
How should I configure the inverter?
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
As the AS-OX has the "0ADJ" potentiometer for frequency meter calibration, use it to adjust the meter so that both readings match.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700