FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency setting
FAQ
Frequency setting
I install an external frequency setting potentiometer externally and connect it to the terminals 10, 2, and 5. And, I use input voltage to set the frequency.
I changed Pr.1 (Maximum frequency) so that the inverter can operate at 100 Hz, but its operation did not change.
How should I configure the setting?
I changed Pr.1 (Maximum frequency) so that the inverter can operate at 100 Hz, but its operation did not change.
How should I configure the setting?
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
Set Pr.125 (Terminal 2 frequency setting gain frequency) instead of Pr.1 (Maximum frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700