FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency manual controller FR-AX
FAQ
Frequency manual controller FR-AX
What is the maximum wiring length between the frequency manual controller FR-AX (with the frequency setting potentiometer, start switch, and frequency meter) and the inverter?
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
Considering voltage drop of the internal power supply and influence by noise, the wiring length should be 30 m or less.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700