FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation stop, frequency setting
FAQ
Operation stop, frequency setting
The inverter does not operate.
I want to stop operation and set frequency with the inverter alone.
I want to stop operation and set frequency with the inverter alone.
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
Set Pr.79 (Operation mode) to "1" (PU operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700