FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > CC-Link
FAQ
CC-Link
In CC-Link operation, I want to input the inverter's operation status into the programmable controller.
I also want to monitor the running frequency and output current values.
I set "H01" and "H02" in the remote register RWwn.
Is it necessary to turn ON the monitor command RYC?
I also want to monitor the running frequency and output current values.
I set "H01" and "H02" in the remote register RWwn.
Is it necessary to turn ON the monitor command RYC?
- Category :
Answer
Turn ON the monitor command RYC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700