FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > CC-Link
FAQ
CC-Link
In CC-Link operation, I want to input the inverter's operation status into the programmable controller.
I want to monitor the running frequency, output current value, and conveyor speed simultaneously.
I want to monitor the running frequency, output current value, and conveyor speed simultaneously.
- Category :
Answer
You cannot monitor the running frequency and conveyor speed (machine speed) simultaneously.
The inverter does not have a function to output them simultaneously.
The inverter does not have a function to output them simultaneously.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700