FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
What is the difference between the CC-Link option FR-A7NC and FR-A7NC E kits?
- Category :
Answer
The FR-A7NC is designed for the FR-A700, FR-F700, and FR-F700P.
The FR-A7NC E kit is designed for the FR-E700 with the dedicated cover. (Only the dedicated cover can fit to it.)
While the optional board itself is the same for all options, the installation method differs from each option. Be sure to follow the correct procedure.
The FR-A7NC E kit is designed for the FR-E700 with the dedicated cover. (Only the dedicated cover can fit to it.)
While the optional board itself is the same for all options, the installation method differs from each option. Be sure to follow the correct procedure.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700