FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency setting
FAQ
Frequency setting
I set the frequency to 40 Hz using the setting dial and operated the inverter.
After resetting the power, should I set the frequency again?
After resetting the power, should I set the frequency again?
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
When the frequency is set using the setting dial, it is not necessary to set it again.
The inverter memorizes the setting value internally even after the power reset.
The inverter memorizes the setting value internally even after the power reset.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700