FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Frequency setting
FAQ
Frequency setting
I set Pr.79 (Operation mode) to "3" (Combined operation mode) and short-circuit the terminals STF and SD from an external source.
If multi-speed selection is ON, changing the frequency using the setting dial does not change the running frequency. Why is this?
If multi-speed selection is ON, changing the frequency using the setting dial does not change the running frequency. Why is this?
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
This is due to specifications that multi-speed selection is prioritized and setting with the setting dial is ignored.
The setting dial is effective when multi-speed selection is OFF.
The setting dial is effective when multi-speed selection is OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700