FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Control terminal
FAQ
Control terminal
Can I use the inverter by connecting the terminals STF and SD and by setting the frequency using the setting dial?
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
You also need to set Pr.79 (Operation mode) to "3".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700