FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Frequency setting
FAQ
Frequency setting
Can I use both of the current input and setting dial on the operation panel to set the frequency?
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
You can use the setting dial together with the terminal 4.
Set Pr.79 (Operation mode) to "3" (Combined operation mode) and assign the AU signal to an unused terminal.
When the terminal AU signal is turned ON, the current input is effective. When the terminal AU signal is turned OFF, the frequency setting with the setting dial on the operation panel is effective.
Set Pr.79 (Operation mode) to "3" (Combined operation mode) and assign the AU signal to an unused terminal.
When the terminal AU signal is turned ON, the current input is effective. When the terminal AU signal is turned OFF, the frequency setting with the setting dial on the operation panel is effective.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700