FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Parameter setting
FAQ
Parameter setting
I want the inverter to start when it has been powered on.
Also, I want to set the frequency using the setting dial.
Which parameter should I set?
Also, I want to set the frequency using the setting dial.
Which parameter should I set?
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
Change Pr.79 (Operation mode) to "3" (Combined operation mode) and short-circuit the external terminals STF and SD (or STR and SD for reverse rotation).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700