Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21861
  • Release Date : 2018/08/22 16:29
  • Print

Setting dial and FR-PA02 built-in potentiometer

I want to use the operation panel FR-PA02 for the FR-E500, but when I connect the inverter and FR-PA02 with a cable, the FR-PA02 becomes active and the operation panel on the inverter becomes inactive.
Can I use the operation panel of the inverter to change the parameter?
Which of the setting dial and the built-in potentiometer of FR-PA02 is effective?
Category : 

Answer

When the FR-PA02 is connected to the inverter with a cable, the FR-PA02 becomes effective.
The operation panel of the inverter can also be used to set some parameters.
For the built-in potentiometer, setting Pr.146 (Built-in potentiometer switching) to "0" enables the potentiometer of the FR-PA02.
Initially, Pr.146 is set to "1" and the potentiometer is inactive.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?