FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA02 built-in potentiometer
FAQ
FR-PA02 built-in potentiometer
How should I configure the setting to use the built-in potentiometer of the operation panel FR-PA02 for the FR-E500?
- Category :
Answer
Change Pr.146 (Built-in potentiometer switching) to "0" (built-in frequency setting potentiometer).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ