Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21870
  • Release Date : 2018/08/22 16:29
  • Print

Operation mode, PU operation mode switching

After changing the parameter setting value, I tried to switch to the PU operation mode and I failed.
I use the FR-A7NC.
Category : 

Answer

Change Pr.340 (Communication startup mode selection) from "1" to "0".
Power OFF and then ON the inverter.
Operate the inverter according to the value of Pr.79 (Operation mode).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?