FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > CC-Link
FAQ
CC-Link
I am considering to control the inverter with the output module and DA conversion unit of the programmable controller using CC-Link. To what extent can I control them from CC-Link communication using the optional FR-A7NC (E kit)?
- Category :
Answer
You can start/stop operation, set the frequency, read/write parameters, and monitor the inverter via CC-Link communication.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700