Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21921
  • Release Date : 2018/08/22 16:30
  • Print

Terminals P1 and P

When using the brake unit FR-BU2, should I remove the jumper between the terminals P1 and P?
Should I set Pr.30 = "0"?
Should I need to set a percent value in Pr.70?
Category : 

Answer

Removal of the jumper between the terminals P1 and P is not necessary unless you are using the DC reactor.
Set Pr.30 = "0" when using the brake unit.
Since setting Pr.30 = "0" invalidates the setting of Pr.70, you do not have to set it.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?