Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21932
  • Release Date : 2018/08/22 16:30
  • Print

Encoder cable length restriction

Can I use the encoder cable FR-VCBL150M for a combination of the FR-V200E (amplifier) and SF-VR (motor)?
Category : 

Answer

If the cable length is longer than 100 m, speed may not be read correctly due to voltage drop and waveform deformation of the encoder signal. Therefore, use the wiring length of up to 100 m.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries