Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21988
  • Release Date : 2018/08/22 16:30
  • Print

Motor heat generation

I use the MM-CF352 (rated current 12.5 A) at around 4 A. (24-hour continuous operation)
The surface temperature is approximately 70 deg C. Is this OK?
Category : 

Answer

The surface temperature of approximately 70?C is OK.
The following shows the MM-CF352 frame temperature for reference.
(Actual temperature rise depends on how the motor is attached.)
- Rated speed (2000 r/min), Under rated load: Around 60 degrees
- Rated speed (2000 r/min), Under no load: Around 30 degrees
If you install the motor where people may touch it, attach a cover to it to prevent the motor from being touched.
Product Name
Inverter, magnet motor drive
Product Category
Motor
Series
Magnetic motor drive
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?