FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Regenerative brake resistor
FAQ
Regenerative brake resistor
Does the FR-E520-0.75K have a built-in brake resistor? What is the inverter's brake torque and duty capabilities without a built-in brake resistor? What is these capabilities with a built-in brake resistor?
- Category :
Answer
The brake resistor is not built in the inverter. Purchase the optional resistor and connect it to the inverter.
Inverter only (without resistor)
Continuous regenerative driving 20% torque
(Not regenerated to the inverter due to a mechanical loss)
FR-ABR-0.75K 10% ED Short-time permissible power 1300 WRS continuous 80WMRS120W100 3% ED Short-time permissible power 560 WRS continuous 30 W
Inverter only (without resistor)
Continuous regenerative driving 20% torque
(Not regenerated to the inverter due to a mechanical loss)
FR-ABR-0.75K 10% ED Short-time permissible power 1300 WRS continuous 80WMRS120W100 3% ED Short-time permissible power 560 WRS continuous 30 W
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500