Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22020
  • Release Date : 2018/08/22 16:30
  • Print

Power factor improving effect by option

If I install the power factor improving converter, AC reactor, DC reactor, line noise filter, and radio noise filter together, how is the power factor improved? Is there any problem by installing all of them?
Category : 

Answer

Installing the high power factor converter brings the power factor improving effect of 99% or higher.
Therefore, when the high power factor converter is used, it is not necessary to install the AC reactor and DC reactor.
Be sure to install the line noise filter and radio noise filter on the input side of the reactor 1 (FR-HCL01: one of the accessories of the high power factor converter).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-S500, FR-E500, FR-A100, FR-F500, FR-A200, FR-A500, FR-V200
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?