FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Winding control
FAQ
Winding control
To wind steel cord processed by a wire drawing machine with an inverter (400 V, 22 kW) the inverter using another inverter with the same capacity, Hitachi provides an applied control device PID-E2DS. Can I implement similar control using the FR-A540?
- Category :
Answer
As an example, you can use an inverter to feed the cord at the constant speed under dancer control using a combination of the deviation detector and deviation sensor, and use a vector inverter's torque control to wind the cord at a constant torque.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500