FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Control circuit power supply
FAQ
Control circuit power supply
Since the FR-A500 series has the control circuit power supply with another terminal, the fault history is retained after a fault occurrence. Is the fault history of the FR-E500 series maintained when the MC trips upon fault occurrence?
- Category :
Answer
If the MC on the input side is shut off using the fault output of the FR-E500, the inverter's fault records are left in the faults history.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500