FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800
FAQ
FR-A800
Is the number of input terminals the same as that of the A700 series?
(For A700: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
(For A700: STF, STR, STOP, RH, RM, RL, JOG, RT, MRS, RES, AU, CS)
- Category :
Answer
Number of terminals: Same input terminals as the A700 series, and the following two terminals are added. Safety: SI1, SI2, SIC 24 V power supply: +24 * The terminals SI1, SI2, and SIC are dedicated to the safety. The function cannot be changed as other terminals.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800