FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Multi-speed setting
FAQ
Multi-speed setting
When Pr.24 (4 speed) of multi-speed setting is only set and RH, RM, RL are all turned ON, which frequency is applied for the operation?
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
If Pr 27 is not set, the operation starts at the speed of RL.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ