Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21238
  • Release Date : 2018/08/22 16:26
  • Print

Remote input signal of CC-Link communication

This is related to the remote input signal (RX1B (remote station ready)) sent from the inverter (FR-A7NC) to the master module. In the Instruction Manual of FR-A7NC, it is described that the signal becomes 0 when the inverter error occurs (protective function operation). If the RES signal turns ON, will the signal be 0?
Category : 

Answer

The signal becomes 0 when the RES signal is turned ON.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries