FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Model setting in FR-Configurator
FAQ
Model setting in FR-Configurator
With the FR-E740, when the automatic recognition is selected in the model setting of FR-Configurator (FR-SW3-SETUP-WJ), "Corresponding inverter does not exist." is displayed.
What are the possible causes?
The recommended connection cable MR-J3USBCBL3M is used.
What are the possible causes?
The recommended connection cable MR-J3USBCBL3M is used.
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
Check the version of FR-Configurator (FR-SW3-SETUP-WJ).
If the version is "1.00", it does not support or detect the FR-E740.
Version "2.00" supports the FR-E740. Upgrade the version from the Mitsubishi Electric FA Global Website.
If the version is "1.00", it does not support or detect the FR-E740.
Version "2.00" supports the FR-E740. Upgrade the version from the Mitsubishi Electric FA Global Website.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700