FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Countermeasure against noises
FAQ
Countermeasure against noises
Can I change the countermeasure against the inverter noise by changing the parameter?
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
Yes.
The carrier frequency can be decreased by the setting of Pr.72 (PWM frequency selection).
The carrier frequency can be decreased by the setting of Pr.72 (PWM frequency selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700