FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Frequency setting
FAQ
Frequency setting
It is described that the initial setting of up to frequency operation range is "10%". Is the up to frequency signal output at 6 Hz when the running frequency is 60 Hz?
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
For the set frequency 60 Hz, ±6 Hz is applied and thus the up to frequency signal is output between 54 Hz and 66 Hz.
During acceleration/deceleration to the allowable range, the signal is turned OFF.
The signal is turned ON during operation within the allowable range.
During acceleration/deceleration to the allowable range, the signal is turned OFF.
The signal is turned ON during operation within the allowable range.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700