FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Current value monitor
FAQ
Current value monitor
Using the monitor functions of the parameter unit, I can display the present value monitor of frequency and voltage values but the current value remains 0.00 A.
I do not think I changed related parameters. What is the possible cause?
I do not think I changed related parameters. What is the possible cause?
- Category :
Answer
The current value can be displayed on the operation panel without regard to the setting of monitor-related parameters.
As the current value remains 0 A, the following causes are probable:
1. The motor and inverter are disconnected and current does not flow into the motor.
2. The motor capacity is extremely smaller than the inverter capacity and the current indicator does not move.
3. Inverter is faulty. Measure the actual current using an ammeter, and if the current is flowing, request us for inspection of the converter.
As the current value remains 0 A, the following causes are probable:
1. The motor and inverter are disconnected and current does not flow into the motor.
2. The motor capacity is extremely smaller than the inverter capacity and the current indicator does not move.
3. Inverter is faulty. Measure the actual current using an ammeter, and if the current is flowing, request us for inspection of the converter.
- Product Name
- Inverter, magnet motor drive
- Series
- Others