Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21452
  • Release Date : 2018/08/22 16:27
  • Print

Difference between FR-AU01 and AU01A

What is the difference between the FR-AU01 and FR-AU01A?
Do you have material for the FR-AU01A (outline dimensions and specifications)?
Category : 

Answer

The major changes from FR-AU01 to FR-AU01A include 1. Case material and 2. Lead wire terminal process method.
The FR-AU01A has a backward compatibility with the FR-AU01 and can be used with the FR-Z220-0.4 to 11k.
For details, refer to the following: Figure 1
Product Name
Inverter, magnet motor drive
Product Category
Manual Controller/Speed controller
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries