FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Control cable between high power factor converter and inverter
FAQ
Control cable between high power factor converter and inverter
Are the high power factor converter and inverter directly connected with a control cable?
Or, is a relay required between them?
Or, is a relay required between them?
- Category :
Answer
Connect the high power factor converter and inverter directly with a control cable, without using a relay. Since a fast-response is required to shut off the inverter output by the RDY signal, and placing a relay delays the response. (Therefore, you can use the relay for the RSO signal.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option