Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21580
  • Release Date : 2018/08/22 16:28
  • Print

Fault output signal when inverter trips

Is there a fault output signal when the inverter trips?
Category : 

Answer

Only the unit type SC-A□□U has fault output signals.
(Terminals Y1 and SD open collector output permissible load 24 VDC 0.1 A)The box type SC-A□□B indicates a fault by blinking the alarm LED on the front panel.
Product Name
Inverter, magnet motor drive
Product Category
Inverter speed controller
Series
SC-A
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?