FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Can I connect it to high power factor converter?
FAQ
Can I connect it to high power factor converter?
Can I connect it to the high power factor converter FR-HC?
- Category :
Answer
It can be connected to an inverter that supports the high power factor converter FR-HC. (It cannot be connected to conventional inverters.)
How to identify inverters supporting the FR-HCInverters of which serial number (indicated on the rating plate of the product) is one of the following or later:
Model???Serial number (Note)
FR-A024-0.1K (P) to 1.5K (P)????B63○○○○○○, Y63○○○○○○
FR-A024-2.2K (P), 3.7K (P)?????P63○○○○○○
FR-A044-0.4K (P), 0.75K (P)?????H63○○○○○○
FR-A044-1.5K (P) to 3.7K (P)?????J63○○○○○○
(Note) If the serial number starts with one of two types of characters, determine from "symbol + year + month".
How to identify inverters supporting the FR-HCInverters of which serial number (indicated on the rating plate of the product) is one of the following or later:
Model???Serial number (Note)
FR-A024-0.1K (P) to 1.5K (P)????B63○○○○○○, Y63○○○○○○
FR-A024-2.2K (P), 3.7K (P)?????P63○○○○○○
FR-A044-0.4K (P), 0.75K (P)?????H63○○○○○○
FR-A044-1.5K (P) to 3.7K (P)?????J63○○○○○○
(Note) If the serial number starts with one of two types of characters, determine from "symbol + year + month".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024