FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Others > Communication option
FAQ
Communication option
Can I use the communication option FR-CU01 with the FR-A200 (E)?
- Category :
Answer
You can remove the parameter unit FR-PU02 and install the FR-CU01 there.
However, since the interface for the parameter unit is used, the communication speed is lower than the computer link plug-in option.
Similarly to the FR-PU02, the FR-CU01 can be installed and removed while the inverter is powered ON.
However, since the interface for the parameter unit is used, the communication speed is lower than the computer link plug-in option.
Similarly to the FR-PU02, the FR-CU01 can be installed and removed while the inverter is powered ON.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-A200