FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency setting
FAQ
Frequency setting
I input the start signal from the terminal STF, and set the frequency using the setting dial. However, neither setting Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode) or turning the setting dial changes the running frequency.
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
Check the setting of Pr.79 (Operation mode).
If the setting value is "2", frequency commands from an external terminal is effective and the frequency setting with the setting dial is disabled.
To enable the frequency setting with the setting dial, set Pr.79 to "3".
If the setting value is "2", frequency commands from an external terminal is effective and the frequency setting with the setting dial is disabled.
To enable the frequency setting with the setting dial, set Pr.79 to "3".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700