Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21846
  • Release Date : 2018/08/22 16:29
  • Print

Setting dial

Can I use the setting dial of the inverter to set the frequency as well as change the parameter values?  
Category : 

Answer

Yes. You can use the setting dial of the inverter to set the frequency as well as change the parameter values.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?