Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21918
  • Release Date : 2018/08/22 16:30
  • Print

Frequency setting

While the FR-E500 has a built-in potentiometer on the operation panel to set the frequency, the FR-E700 has the setting dial only. How can I set the frequency?  
Category : 

Answer

Use the setting dial to set the frequency with the FR-E700.
You can also use the setting dial to set the parameters.
(By setting Pr.161, you can use the setting dial as a potentiometer.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries