Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22036
  • Release Date : 2018/08/22 16:30
  • Print

Position control

I am considering how to control positioning of equipment that moves horizontally.
What are the pros and cons of using vector inverter, servo motor, and stepping motor?
Category : 

Answer

The servo motor provides the highest precision and response.

With the vector inverter, position control using pulse train input ensures position control at precision of encoder resolution ±1 pulse.
However, since the motor inertia is large, the response is lower than the servo motor.
The stepping motor uses open-loop control and precision equivalent to the servo motor cannot be expected, and also loss in synchronism may occur.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries