FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Phase detection terminal
FAQ
Phase detection terminal
I cannot find the terminal block for the FR-RC-15K's phase detection terminal.
Where is the phase detection terminal (TB1-5)?
I found all other terminals.
Where is the phase detection terminal (TB1-5)?
I found all other terminals.
- Category :
Answer
The phase detection terminal has been provided with units produced since December 1999.
You can identify these units with the serial number "N9Z○○○○○○" or later.
"N" is a symbol for the unit, "9" following it represents the year 1999, and "Z" represents December.
If your unit does not have the phase detection terminal, use the conventional wiring method.
You can identify these units with the serial number "N9Z○○○○○○" or later.
"N" is a symbol for the unit, "9" following it represents the year 1999, and "Z" represents December.
If your unit does not have the phase detection terminal, use the conventional wiring method.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power regeneration converter
- Series
- Option