FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A100 > Compatibility of the function with FR-A100
FAQ
Compatibility of the function with FR-A100
Are the functions of the FR-A100EXCELLENT and FR-A100 compatible?
- Category :
Answer
Yes.
Compared with the FR-A100:- The PI control function is added.- Fast-response current limit operation is improved.- Cumulative energy monitor is added.
Compared with the FR-A100:- The PI control function is added.- Fast-response current limit operation is improved.- Cumulative energy monitor is added.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100