FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Frequency setting
FAQ
Frequency setting
Is it always necessary to set the frequency for inverter operation?
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
Yes.
The inverter requires the start signal and frequency setting signal.
The inverter requires the start signal and frequency setting signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700